iglidur® - Coefficients of friction


Coefficients of friction under different loads A = low load
B = high load
 
Coefficients of friction under different loads
Coefficients of friction of the iglidur plain bearings at the recommended shaft surface finish and low load Coefficients of friction of the iglidur plain bearings at the recommended shaft surface finish and low load, p = 0.75 MPa
iglidur plain bearings are self-lubricating with the addition of solid lubricants. The solid lubricants lower the coefficient of friction of the plain bearings and thus increase the wear resistance. The coefficient of friction μ is proportional to the normal force and describes which force is needed to move a body in relation to another. Depending on whether an application is starting from a stationary position or the movement is in progress and needs to be maintained, a distinction is made between a static coefficient of friction and a dynamic coefficient of friction.

Coefficients of friction and surfaces

Shown here is the relationship between coefficient of friction and surface finish of shaft materials. It is clearly shown that the amount of friction is composed of different factors.
 
If the shaft is too rough, abrasion levels play an important role. Small areas of unevenness that can interlock with each other must be worn off the surface. When the surfaces are too smooth, however, higher adhesion results, i.e. the surfaces stick to each other. Higher forces are necessary to overcome the adhesion, which results from an increased coefficient of friction. Stick-slip can be the result of a large difference between static and dynamic friction and of a higher adhesive tendency of mating surfaces. Stick-slip also occurs due to intermittent running behaviour and can result in loud squeaking. Over and over again, it is observed that these noises do not occur or can be eliminated with rough shafts. Thus for applications that have a great potential for stick-slip - slow movements, large resonance of the housing - attention must be paid to the optimal surface finish of the shafts.
 
Friction analysis in the igus laboratory Friction analysis in the igus laboratory

Consulting

I look forward to answering your questions

Photo
Aw Kai Hua

Product Manager for iglidur® Bearings ASEAN

Write e-mail

Shipping and consultation

In person:

Monday to Friday from 8:30 am - 5:30 pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH