Conveyor rollers

With the ever-increasing requirements in conveyor technology, especially material handling, the demands on the materials used in the conveyed goods to be transported are also increasing. With increasing speed, one of the most important elements in drive technology must function reliably: the bearing. Conveyor rollers are available in a wide variety of designs: driven conveyor rollers made of steel, stainless steel, aluminium or plastic. They are there to establish rolling contact between the conveyor frame and the conveyor belt.
xiros conveyor roller made of aluminium
In principle, conveyor rollers consist of a supporting axis enclosed by a supporting jacket, as well as deep groove ball bearings with flanges as end caps. Our conveyor rollers for roller conveyors can be used flexibly and can be equipped with different deep groove ball bearings depending on requirements. In addition to conveyor technology, xiros conveyor rollers with ball bearings are used in labelling technology, packaging and the food industry, where they can also take on the function of a guide roller.
Everything about our conveyor rollers at a glance:

What are the advantages of our conveyor rollers?

Icon: lubrication-free

Lubrication-free

The plastic ball bearings used are lubrication-free and require no further lubrication with grease. This means that the conveyor roller does not have to overcome the resistance of the lubricant and always runs smoothly. You achieve savings in three ways: with regard to maintenance, weight and price.
Polymer ball bearings direct from the manufacturer

Directly from the manufacturer

xiros plastic ball bearings are the result of our own efforts and work. You not only benefit from an immense variety directly from the manufacturer, for example compared to solutions as heavy steel, but also from years of experience from the industry's largest test laboratory for motion plastics.
Icon: FDA-compliant

Food-compatible

Some of our conveyor rollers can be used safely in the food and beverage industry. They are resistant to chemicals such as fatty acids or grease. This is certified by the European Commission with Regulation 10/2011/EU based on Regulation 1935/2004/EC.

Where can I buy the conveyor rollers?

Buy conveyor rollers
You can find a wide selection of our conveyor rollers in our online shop: diameters from 20 to 100mm and lengths of up to 1,500mm
  • Aluminium conveyor rollers: clear anodised, black anodised, sandblasted, non-stick coated
  • Stainless steel conveyor rollers: FDA-compliant, antistatic and for high-temperature applications
  • PVC conveyor rollers: FDA-compliant and completely metal-free
  • Conveyor rollers made of carbon: thin-walled and optionally available as an antistatic version

▷ Buy conveyor rollers in the online shop

Configure conveyor rollers online

With the online tool for configuring xiros conveyor rollers, you will receive the right product in just a few steps after entering your requirements. Simply enter the outer and inner diameter, determine the load and load case as well as the temperature of the application.▷ Configure conveyor rollers online
Configure and order conveyor rollers online

Choosing the right conveyor roller

White paper: Seven tips for choosing the right conveyor rollers Our free white paper will help you select the ideal conveyor roller for your individual application.

▷ Seven tips for choosing the right conveyor roller
There are several factors to consider when selecting conveyor rollers. First of all, load-bearing capacity is a decisive criterion. The conveyor roller must be able to safely bear the weight of the transported goods without deforming, sustaining damage or causing downtime. The durability of the conveyor rollers is also of great importance. They should be made of materials with high wear resistance to ensure a long service life.

Rolling friction must also not be ignored. The conveyor rollers should have an optimum surface finish to ensure sufficient grip on the conveyor belt or the transported goods. This contributes to the stability and safety of the conveying process. Ease of installation and maintenance also play a role, as downtimes of the entire conveyor system are thus avoided.

Where are conveyor rollers used?


Consulting

I look forward to answering your questions

Photo
Zhao Ming Luo

Product Manager

Write e-mail

Shipping and consultation

In person:

Monday to Friday from 8:30 am - 5:30 pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH