igus® Slewing Ring Ball Bearings: Precision, Durability, and Maintenance-Free Operation

Slewing ring ball bearings, also known as turnable bearings, are a specific type of large bearing designed to handle simultaneous axial and radial forces. These bearings differ from traditional ball bearings as they are not housed within a casing or mounted on a shaft. Instead, they feature mounting holes on both the inner and outer rings, facilitating efficient power transmission and swift integration with adjacent components. Typically, these bearings are stacked during assembly, although vertical installation is also feasible. The rolling elements within metal slewing ring ball bearings are spaced apart and travel along a raceway that is both sealed and lubricated. igus a company in this field, provides two distinct types of 100% lubrication-free slewing ring ball bearings. One type operates on low-maintenance sliding elements, while the other is supported by ball bearings. These can be further customized with options such as outer drive teeth, inner drive teeth, or specialized parts tailored to specific requirements.

iglidur PRT slewing ring ball bearing supported by plain bearings

 
  • 100% lubrication-free
  • Very slim design
  • Ready-to-install & easy to assemble
  • Resistant to dirt, dust, corrosion and humidity
  • Individually configurable
Find out more

xiros slewing ring ball bearing supported by ball bearings

 
  • 100% lubrication-free
  • Available as a completely metal-free version
  • Ideal for the food and chemical industries
  • FDA-compliant components
Find out more

Our slewing ring ball bearings in use

Assembly table with PRT slewing ring bearing

Assembly table with iglidur PRT-01 slewing ring bearing

"We were looking for a simple slewing ring bearing that would allow our assembly table to rotate. Using the maintenance-free PRT slewing ring bearings was therefore very helpful, and the cooperation with igus went very well."
Maciej Banaś, GBK Projektowanie i Budowa Maszyn
More on the application
EasyCure heating cable drum from Bodenbender GmbH

Heating cable drum with xirodur B180 slewing ring ball bearing

"The xiros slewing ring ball bearings impressed us due to their lack of lubrication, smooth running and low weight of the plastic. The individual design options for the products were also very helpful during the development process."
Jonas Bodenbender, CEO Bodenbender GmbH
More on the application

Our new products in the area of slewing ring ball bearings



The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus SE & Co. KG or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® SE & Co. KG